At-a-glance
The client is one of the leading cement suppliers, headquartered in Europe, and as of 2018 was one of the top 5 largest providers in the world. With an estimated total capacity of upwards of 300M-ton/yr for that year and over 200 integrated cement plants worldwide, the client is looking for ways to improve the efficiency of its kilns in order to improve customer experience, maximize its revenue, save on costs and maximize its cash flows.
The challenge
With that objective in mind, the client approached SKF’s Enlight AI division to tackle a well-known problem that frequently causes unscheduled downtime in its factories: the buildup and collapse of rings of the rotary kiln.
Once this ring collapses inside the kiln it then progresses forward into the crusher. The clinker crusher is immediately blocked and the kiln becomes inoperable until engineers have cleaned the clinker crusher.

On average, a typical cement factory experiences over 9 kiln breakdowns per year because of this issue, resulting in more than 3 days of production downtime in total and accruing high maintenance overtime costs.
To reduce the overall number of clinker-crusher stoppages, the client specifically wanted to be able to identify proactively when the rings were being formed in the kiln in real-time. Armed with this knowledge, plant engineers would be able to make changes to the oven’s temperature, prevent the formation of further rings and avoid machine downtime altogether.
The business problem
- Lost production/revenue due to unscheduled kiln downtime of +9 per year per factory
- High O&M costs from overtime labor expenditures
The solution
The client chose 2 reference factories to pilot the SKF Enlight AI Predictive Analytics model. During the trial period data generated by dozens of sensors was streamed to Enlight AI’s cloud where it was processed by Enlight’s advanced Machine Learning algorithms (AutoML).
Based on detection of subtle anomalous and indicative behavioral patterns, the solution provided predictive alerts of evolving ring formations within the kiln.
The results
- Quality Prediction Rate: 94%
- Time to Failure: ~2 days
The bottom line
SKF Enlight AI was able to accurately predict 94% of the formation of residual rings within the kilns, effectively enabling engineers to make the necessary modifications to stop more rings from materializing and to prevent crusher and process stoppages due to these rings.
Business impact/ROI
Once SKF Enlight AI is fully deployed the plant expects to see a 30% reduction in unplanned downtime leading to annual savings of millions of Euros.
Industrial plants generate terabytes of process data. SKF Enlight AI is a SaaS Predictive Maintenance solution that uses Automated Machine Learning to identify emerging asset failure patterns within this data. It provides early warnings and sensor-level intelligence to help avert unplanned downtime and meet production goals. For more information on how SKF Enlight AI can improve performance and reliability, click here.